8.3.3 Defsym Option
The --defsym
sym=expr option defines a symbol.
This option creates a global symbol in the output file, containing the
absolute address given by expr. You may
use this option as many times as necessary to define multiple symbols in the command line.
A limited form of arithmetic is supported for the expr in this context: you may give a hexadecimal constant or the
name of an existing symbol, or use + and - to add or
subtract hexadecimal constants or symbols.
Note: There should be no white space between
sym, the equals sign (=) and
expr.