10.1.6 Building the Output File
Finally, the linker builds the output file. Relocation entries in each section are patched using absolute addresses. If the address computed for a symbol does not fit in the relocation entry, a link error results. This can occur, for example, when one module references a variable which it thinks is in a “small data” section, while the other defines it in a non-small section.
A link map is also generated if requested with the -Map linker option. The link map includes a memory usage report, which shows the starting address and length of all sections in data memory and program memory. An additional memory-usage report by module is included, which shows the memory usage of each input object in the final ELF output. For more information about the link map, see Map File.