12.2.9 M
Macros nested too deeply.
The maximum macro nesting depth is 10.
May not nest groups (--help for usage).
An archive group is already started. Use the -) option to close the current group before starting another group with the -( option.
Member %b in archive is not an object.
The archive member is not a valid object. Check that the library archive is correct for the Microchip MPLAB XC32 C/C++ Compiler.
Missing argument(s) to option --section-start.
The required argument to --section-start
must be sectionname=org.
Multiple definition of name.
The linker discovered a symbol that is defined multiple times. Eliminate the extraneous definition(s).
Multiple startup files.
The linker script is attempting to set a startup file, but a startup file has already been set. There should be only one startup file specified in the linker script.