12.2.2 A
A heap is required, but has not been specified.
A heap must be specified when using Standard C input/output functions.
Assignment to location counter invalid outside of SECTION.
An assignment to the special dot symbol can be done only during allocation within a SECTION. Check the location of the assignment statement in the linker script.