3.6.3.1.15 TrustZone Basic Demonstration on PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit
Description
This example application performs how to Add and Multiply Math operations in secure mode and I/O operations in non-secure mode.This demonstrates TrustZone feature and uses two projects viz., Secure and Non-Secure Project that work together on the same MCU and offering security isolation between the Trusted and the Non-trusted resources in the device.
- Secure project implements math functions (add and multiply as example).
- Non-secure project uses the math functions exposed by secure project for math operations.
Modules/Technology Used
- Peripheral Modules
- SERCOM3 (USART)
- PM
- EVSYS
- NVMCTRL
- PORT
The MCC Harmony project graph would look like this:
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware\trustzone_basic\src\config\pic32cm_ls00_cnano.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the PIC32CM LS00
Curiosity Nano+ Touch Evaluation Kit to the Host PC as a USB Device
through a Type-A male to micro-B USB cable connected to Micro-B USB
(Debug USB) port.

Programming hex file
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File
- In the Import Image
File window,
- Create Prebuilt
Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as PIC32CM5164LS00048.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project
Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt
Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (trustzone_basic\firmware\trustzone_basic) in MPLAB X IDE.
- Ensure PIC32CM LS00 Curiosity Nano is selected as hardware tool to program/debug the application.
- Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar.
- Follow the steps in Running the Demo section below.
Running the Demo
- Open the Tera Term/PuTTY terminal application on the PC (from the Windows® Start menu by pressing the Start button).
- Set the baud rate to 115200 and enable the Local echo by selecting setup > Terminal > Local echo.
- To Reset the device, run
this command: ipecmd.exe -P32CM5164LS00048 -TPNEDBG -OK from the
following location: C:\Program
Files\Microchip\MPLABX\v6.20\mplab_platform\mplab_ipe.
Note: The PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit does not include a reset button. Therefore, the device can be reset by executing the reset command in the CMD prompt. - The following message is
displayed on the serial terminal.

Tera Term Output
Perform the following sequence of operations to do addition of two numbers:
- Press 'a' to start an addition operation.
- Enter a 16 bit unsigned integer and press Enter on keyboard.
- Enter second 16 bit unsigned number and press Enter on keyboard.
- Observe the result which is addition of first and second 16 bit unsigned number.
Perform the following sequence of operations to do multiplication of two numbers:
- Press 'b' to start an addition operation.
- Enter a 16 bit unsigned integer and press Enter on keyboard.
- Enter second 16 bit unsigned number and press Enter on keyboard.
- Observe the result which is
multiplication of first and second 16 bit unsigned number,

Comments
- Reference Training Module: Arm TrustZone Getting Started Application on PIC32CM LS60 (Arm Cortex-M23) MCUs
- This application demo
builds and works out of box by following the instructions above in
Running the Demo section. If the user needs to
enhance/customize this application demo, should use the MPLAB Harmony v3
Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project