3.9.4.1.14 TCC PWM Generation on PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit

Download

Description

This application example shows how to use Timer Counter for Control Applications (TCC) module to generate PWM signals. The TCC is configured to generate synchronous 2 or 3 phase PWM signals with dead time. The duty cycle of the PWM signals is updated in the period interrupt handler.

Modules/Technology Used

  • Peripheral Modules
    • TCC0
    • PM
    • EVSYS
    • NVMCTRL
    • PORT
    The following figure provides the MCC Harmony project graph with all the components.

Hardware Used

Software/Tools Used

This project has been verified to work with the following versions of software tools:

Refer to the Project Manifest present in harmony-manifest-success.yml under the project folder firmware\tcc_timer_mode\src\config\pic32cm_ls00_cnano.

  • Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version

Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).

Setup

  • Connect the PIC32CM LS00 Curiosity Nano+ Touch evaluation kit to the host PC as a USB device through a Type-A male to micro-B USB cable connected to Micro-B USB (Debug USB) port
  • To establish the connection with the Saleae Logic Analyzer to the host PC
    Table 3-1. Pin Details
    Signal NamePad
    ch0-PWMHPA08
    ch0-PWMLPA09
    ch1-PWMHPA10
    ch1-PWMLPA14
    ch2-PWMHPA15
    ch2-PWMLPA16

Programming Hex File

The pre-built hex file can be programmed by following the below steps.

Steps to program the hex file
  • Open MPLAB X IDE
  • Close all existing projects in IDE, if any project is opened
  • Go to File>Import>Hex/ELF File
  • In the Import Image File window,
    1. Create Prebuilt Project,
      • Click the Browse button to select the prebuilt hex file
      • Select Device as PIC32CM5164LS00048
      • Ensure the proper tool is selected under Hardware Tool and click the Next button
    2. Select Project Name and Folder,
      • Select appropriate project name and folder and click the Finish button
  • In MPLAB X IDE, click the Make and Program Device button to program the device

Programming/Debugging Application Project

  • Open the project (tcc_synchronous_pwm_channels\firmware\tcc_timer_mode) in MPLAB X IDE
  • Ensure PIC32CM LS00 Curiosity Nano is selected as hardware tool to program/debug the application
  • Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
  • Follow the steps in Running the Demo section

Running the Demo

  • Open the Saleae logic application on the PC (from the Windows® Start menu by pressing the Start button).
  • Observe the PWM frequency to be 10 kHz

Logic Analyzer Output

  • The following high-side and low-side PWM waveforms are displayed on the Logic Analyzer
  • Observe the dead time between the high side and the low side.

Comments