3.9.4.1.11 SERCOM SPI EEPROM Read Write on PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit
Description
This example shows how to use the SPI peripheral to write an array of values to the SPI Serial EEPROM and verify the value written by reading the values back and comparing it to the value written and the LED indicates the success or failure by turning ON and OFF the LED (LED1) on the PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit.
Modules/Technology Used
- Peripheral Modules
- SERCOM1 (SPI)
- PM
- EVSYS
- NVMCTRL
- PORT
The following figure provides the MCC Harmony project graph with all the components.
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer to the Project Manifest present in
harmony-manifest-success.yml under the project folder
firmware\spi_eeprom_write_read\src\config\pic32cm_ls00_cnano.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the PIC32CM LS00 Curiosity
Nano+ Touch Evaluation Kit to the host PC as a USB device through a Type-A male to
micro-B USB cable connected to Micro-B USB (Debug USB) port
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to
File>Import>Hex/ELF File - In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CM5164LS00048
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project Name and Folder,
- Select appropriate project name and folder and click the Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click the Make and Program Device button to program the device
Programming/Debugging Application Project
- Open the project
(
spi_eeprom_write_read\firmware\spi_eeprom_write_read) in MPLAB X IDE - Ensure
PIC32CM LS00 Curiosity Nanois selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
Output
- The LED is turned ON when the value read from the EEPROM matched with the written value
- The LED is turned OFF when the value
read from the EEPROM did not match with the written value
Comments
- Reference Training Module: Arm TrustZone Getting Started Application on PIC32CM LS60 (Arm Cortex-M23) MCUs
- This application demo builds and
works out of box by following the instructions in Running the Demo section. If the
user needs to enhance/customize this application demo, should use the MPLAB Harmony v3
Software framework. Refer to the following links to setup and build the applications
using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project