3.2.8.4 Provisioning Service
The provisioning service helps to configure the Wi-Fi interface credentials. It
supports TCP tunnel and Web server based provisioning services. It implements or handles
all the required AT commands to start the module in Access Point mode and open up a TCP
tunnel or serve a HTML web page to receive the Wi-Fi credentials. The provisioning
service call API syntax is provided below:
SYS_RNWF_RESULT_t SYS_RNWF_PROV_SrvCtrl(SYS_RNWF_PROV_SERVICE_t request, SYS_RNWF_WIFI_PROV_HANDLE_t);This
section allows the following configurations:- Provision Debug logs : Enable to get the provision service logs.
- Provision Callback Handler: Configure callback function name for Wi-Fi Provisioning states
Provisioning Service Configuration in MCC
The provisioning service provides the following options for the user:
The following list captures the provisioning service callback event codes and
their arguments
| Options | Inputs | Remarks |
|---|---|---|
SYS_RNWF_PROV_ENABLE | None | Enables the provisioning service |
SYS_RNWF_PROV_DISABLE | None | Disables the provisioning service |
SYS_RNWF_PROV_SET_CALLBACK | Callback handler | Registers the application callback function to report the provisioning status |
| Event | Response Components | Remarks |
|---|---|---|
SYS_RNWF_PROV_COMPLTE | Mode, SSID, Passphrase, Security, Autoenable | Provisioning complete and returns the provisioned Access Point credentials. User application can store it securely for auto reconnection on every boot up |
SYS_RNWF_PROV_FAILURE | None | Provisioning failure |
The following figure illustrates the Provisioning service sequence.
The following example code showcases the use of provisioning
service:
/*
Provisioning application
*/
// *****************************************************************************
// *****************************************************************************
// Section: Included Files
// *****************************************************************************
// *****************************************************************************
#include <string.h>
#include <stdio.h>
#include <stddef.h>
#include <stdbool.h>
#include <stdlib.h>
/* This section lists the other files that are included in this file.*/
#include "app_rnwf02.h"
#include "user.h"
#include "definitions.h"
#include "configuration.h"
#include "system/debug/sys_debug.h"
#include "system/inf/sys_rnwf_interface.h"
#include "system/net/sys_rnwf_net_service.h"
#include "system/sys_rnwf_system_service.h"
#include "system/wifi/sys_rnwf_wifi_service.h"
#include "system/wifiprov/sys_rnwf_provision_service.h"
// *****************************************************************************
// *****************************************************************************
// Section: Global Data Definitions
// *****************************************************************************
// *****************************************************************************
// *****************************************************************************
// *****************************************************************************
/* Application Data
Summary:
Holds application data
Description:
This structure holds the application's data.
Remarks:
This structure should be initialized by the APP_Initialize function.
Application strings and buffers are be defined outside this structure.
*/
/*Shows the application's current state*/
static APP_DATA g_appData;
/* Variable to check the UART transfer */
static volatile bool g_isUARTTxComplete = true;
/*Application buffer to store data*/
static uint8_t g_appBuf[SYS_RNWF_IF_LEN_MAX];
// *****************************************************************************
// *****************************************************************************
// Section: Application Local Functions
// *****************************************************************************
// *****************************************************************************
/* DMAC Channel Handler Function */
static void APP_RNWF_usartDmaChannelHandler ( DMAC_TRANSFER_EVENT event, uintptr_t contextHandle)
{
if (event == DMAC_TRANSFER_EVENT_COMPLETE)
{
g_isUARTTxComplete = true;
}
}
/* Application Wifi Callback Handler function */
static void SYS_RNWF_WIFI_CallbackHandler ( SYS_RNWF_WIFI_EVENT_t event, SYS_RNWF_WIFI_HANDLE_t wifiHandler)
{
uint8_t *p_str = (uint8_t *)wifiHandler;
switch(event)
{
/* Wi-Fi connected event code*/
case SYS_RNWF_WIFI_CONNECTED:
{
SYS_CONSOLE_PRINT("Wi-Fi Connected \r\n");
break;
}
/* Wi-Fi disconnected event code*/
case SYS_RNWF_WIFI_DISCONNECTED:
{
SYS_CONSOLE_PRINT("Wi-Fi Disconnected\nReconnecting... \r\n");
SYS_RNWF_WIFI_SrvCtrl(SYS_RNWF_WIFI_STA_CONNECT, NULL);
break;
}
/* Wi-Fi DHCP complete event code*/
case SYS_RNWF_WIFI_DHCP_IPV4_COMPLETE:
{
SYS_CONSOLE_PRINT("IPv4 DHCP Done...%s \r\n",&p_str[2]);
break;
}
/* Wi-Fi IPv6 Local DHCP complete event code*/
case SYS_RNWF_WIFI_DHCP_IPV6_LOCAL_COMPLETE:
{
SYS_CONSOLE_PRINT("IPv6 Local DHCP Done...%s \r\n",&p_str[2]);
/*Local IPv6 address code*/
break;
}
/* Wi-Fi IPv6 Global DHCP complete event code*/
case SYS_RNWF_WIFI_DHCP_IPV6_GLOBAL_COMPLETE:
{
SYS_CONSOLE_PRINT("IPv6 Global DHCP Done...%s \r\n",&p_str[2]);
/*Global IPv6 address code*/
break;
}
default:
{
break;
}
}
}
/* Application Wifi Provision Callback handler */
static void SYS_RNWF_WIFIPROV_CallbackHandler ( SYS_RNWF_PROV_EVENT_t event,SYS_RNWF_WIFI_PROV_HANDLE_t wifiProvHandler)
{
uint8_t *p_str = (uint8_t *)wifiProvHandler;
switch(event)
{
/**<Provisionging complete*/
case SYS_RNWF_PROV_COMPLTE:
{
SYS_RNWF_PROV_SrvCtrl(SYS_RNWF_PROV_DISABLE, NULL);
SYS_RNWF_WIFI_SrvCtrl(SYS_RNWF_WIFI_SET_CALLBACK, SYS_RNWF_WIFI_CallbackHandler);
// Application can save the configuration in NVM
SYS_RNWF_WIFI_SrvCtrl(SYS_RNWF_SET_WIFI_PARAMS, (void *)p_str);
break;
}
/**<Provisionging Failure*/
case SYS_RNWF_PROV_FAILURE:
{
break;
}
default:
{
break;
}
}
}
/* Application Initialization function */
void APP_RNWF02_Initialize ( void )
{
/* Place the App state machine in its initial state. */
g_appData.state = APP_STATE_INITIALIZE;
}
/* Maintain the application's state machine. */
void APP_RNWF02_Tasks ( void )
{
switch(g_appData.state)
{
/* Application's state machine's initial state. */
case APP_STATE_INITIALIZE:
{
DMAC_ChannelCallbackRegister(DMAC_CHANNEL_0, APP_RNWF_usartDmaChannelHandler, 0);
SYS_RNWF_IF_Init();
g_appData.state = APP_STATE_REGISTER_CALLBACK;
break;
}
/* Register the necessary callbacks */
case APP_STATE_REGISTER_CALLBACK:
{
SYS_RNWF_SYSTEM_SrvCtrl(SYS_RNWF_SYSTEM_GET_MAN_ID, g_appBuf);
SYS_CONSOLE_PRINT("\r\nManufacturer = %s\r\n", g_appBuf);
SYS_RNWF_SYSTEM_SrvCtrl(SYS_RNWF_SYSTEM_SW_REV, g_appBuf);
SYS_CONSOLE_PRINT("\r\nSoftware Revision:- %s\r\n", g_appBuf);
SYS_RNWF_SYSTEM_SrvCtrl(SYS_RWWF_SYSTEM_GET_WIFI_INFO, g_appBuf);
SYS_CONSOLE_PRINT("\r\nWi-Fi Info:- \r\n%s\r\n", g_appBuf);
/* Set Regulatory domain/Country Code */
const char *regDomain = SYS_RNWF_COUNTRYCODE;
SYS_CONSOLE_PRINT("\r\nSetting regulatory domain : %s\r\n",regDomain);
SYS_RNWF_WIFI_SrvCtrl(SYS_RNWF_WIFI_SET_REGULATORY_DOMAIN, (void *)regDomain);
// Enable Provisioning Mode
SYS_RNWF_PROV_SrvCtrl(SYS_RNWF_PROV_ENABLE, NULL);
SYS_RNWF_PROV_SrvCtrl(SYS_RNWF_PROV_SET_CALLBACK, (void *)SYS_RNWF_WIFIPROV_CallbackHandler);
g_appData.state = APP_STATE_TASK;
break;
}
/* Run Event handler */
case APP_STATE_TASK:
{
SYS_RNWF_IF_EventHandler();
break;
}
default:
{
break;
}
}
}
/*******************************************************************************
End of File
*/