1.4.2 Park Transform
The stator current is represented on a two-axis orthogonal system with the axis called α-β. The next step is to transform this into another two-axis system that is rotating with the rotor flux. This transformation uses the Park Transform, as illustrated in the following figure. This two-axis rotating coordinate system is called the d-q axis. θ represents the rotor angle.