1.4.3 Inverse Park

After the PI iteration, there are two voltage component vectors in the rotating d-q axis. The user will need to go through complementary inverse transforms to get back to the three-phase motor voltage. First, transform from the two-axis rotating d-q frame to the two-axis stationary frame α-β. This transformation uses the Inverse Park Transform, as illustrated in the following figure.

Figure 1-6. Inverse Park Transform