1.4.4 Inverse Clarke

The next step is to transform from the stationary two-axis α-β frame to the stationary three-axis, Three-phase reference frame of the stator. Mathematically, this transformation is accomplished with the Inverse Clark Transform, as illustrated in the following figure.

Figure 1-7. Inverse Clark Transform