32.5.9 Double Sample Conversion

Double sampling is enabled by setting the ADDSEN bit. When this bit is set, two conversions are required before the module will calculate threshold error. Each conversion must still be triggered separately when ADCONT = 0. The first conversion will set the ADMATH bit and update ADACC, but will not calculate ADERR or trigger ADTIF. When the second conversion completes, the first value is transferred to ADPREV (depending on the setting of ADPSIS) and the value of the second conversion is placed into ADRES. Only upon the completion of the second conversion is ADERR calculated and ADTIF triggered (depending on the value of ADCALC).