32.2.7 ADC Conversion Procedure (Basic Mode)
This is an example procedure for using the ADC to perform an Analog-to-Digital Conversion:
- Configure the Port:
- Disable the pin output driver (Refer to the TRISx register)
- Configure the pin as analog (Refer to the ANSELx register)
- Configure the ADC module:
- Select the ADC conversion clock
- Configure the voltage reference
- Select the ADC input channel (precharge+acquisition)
- Turn on ADC module
- Configure the ADC interrupt (optional):
- Clear the ADC interrupt flag
- Enable the ADC interrupt
- Enable the peripheral interrupt (PEIE bit)
- Enable the global interrupt (GIE bit)(1)
- If ADACQ =
0
, software must wait the required acquisition time(2). - Start the conversion by setting the ADGO bit.
- Wait for the ADC conversion to complete by one of the
following:
- Polling the ADGO bit
- Waiting for the ADC interrupt (interrupts enabled)
- Read the ADC Result.
- Clear the ADC interrupt flag (required if interrupt is enabled).
Important:
- With global interrupts disabled, the device will wake from Sleep but will not enter an Interrupt Service Routine.
- Refer to 32.3 ADC Acquisition Requirements.
ADC Conversion (assembly)
; This code block configures the ADC for polling, Vdd and Vss references, ; FRC oscillator, and AN0 input. ; Conversion start & polling for completion are included. BANKSEL ADCON1 clrf ADCON1 ; clrf ADCON2 ; Legacy mode, no filtering, ADRES->ADPREV clrf ADCON3 ; no math functions clrf ADREF ; Vref = Vdd & Vss clrf ADPCH ; select RA0/AN0 clrf ADACQ ; software controlled acquisition time clrf ADCAP ; default S&H capacitance clrf ADRPT ; no repeat measurements clrf ADACT ; auto-conversion disabled movlw B'10010100' ; ADC On, right-justified, FRC clock movwf ADCON0 BANKSEL TRISA ; bsf TRISA,0 ; Set RA0 to input BANKSEL ANSEL ; bsf ANSEL,0 ; Set RA0 to analog call SampleTime ; Acquisiton delay BANKSEL ADCON0 bsf ADCON0,ADGO ; Start conversion btfsc ADCON0,ADGO ; Is conversion done? goto $-2 ; No, test again BANKSEL ADRESH ; movf ADRESH,W ; Read upper 2 bits movwf RESULTHI ; store in GPR space movf ADRESL,W ; Read lower 8 bits movwf RESULTLO ; Store in GPR space
ADC Conversion (C)
/*This code block configures the ADC for polling, VDD and VSS references, ADCRC oscillator and AN0 input. Conversion start & polling for completion are included. */ void main() { //System Initialize initializeSystem(); //Setup ADC ADCON0bits.FM = 1; //right justify ADCON0bits.CS = 1; //FRC Clock ADPCH = 0x00; //RA0 is Analog channel TRISAbits.TRISA0 = 1; //Set RA0 to input ANSELAbits.ANSELA0 = 1; //Set RA0 to analog ADCON0bits.ON = 1; //Turn ADC On while (1) { ADCON0bits.GO = 1; //Start conversion while (ADCON0bits.GO); //Wait for conversion done resultHigh = ADRESH; //Read result resultLow = ADRESL; //Read result } }