32.2.1 Starting a Conversion
To enable the ADC module, the ADON must be set to a ‘1’. A conversion may be started by any of the following:
- Software setting the ADGO bit to ‘1’
- An external trigger (source selected by ADACT32.7.22 ADACT)
- A continuous-mode retrigger (see section 32.5.8 Continuous Sampling Mode)
.
Important: The ADGO bit must not be set in the same
instruction that turns on the ADC. Refer to 32.2.7 ADC Conversion Procedure (Basic Mode).