1.1.3.6.4 DRV_GENERICCODEC_MicMuteOn Function
void DRV_GENERICCODEC_MicMuteOn(DRV_HANDLE handle);Summary
Mutes the Generic Codec's microphone input
Description
This function mutes the Generic Codec's microphone input
Preconditions
The DRV_GENERICCODEC_Initialize routine must have been called for the specified Generic Codec driver instance.
DRV_GENERICCODEC_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
None.
Example
_// myAppObj is an application specific object._ MY_APP_OBJ myAppObj; _// myGENERICCODECHandle is the handle returned // by the DRV_GENERICCODEC_Open function._ DRV_GENERICCODEC_MicMuteOn(myGENERICCODECHandle); _//Generic Codec microphone muted_
C
void DRV_GENERICCODEC_MicMuteOn(DRV_HANDLE handle);