1.1.3.6.8 DRV_GENERICCODEC_SamplingRateSet Function
void DRV_GENERICCODEC_SamplingRateSet(DRV_HANDLE handle, uint32_t samplingRate)Summary
This function sets the sampling rate of the media stream.
Description
This function sets the media sampling rate for the client handle.
Preconditions
The DRV_GENERICCODEC_Initialize routine must have been called for the specified Generic Codec driver instance.
DRV_GENERICCODEC_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| samplingRate | Sampling frequency in Hz |
Returns
None.
Remarks
None.
Example
_// myGENERICCODECHandle is the handle returned // by the DRV_GENERICCODEC_Open function._
DRV_GENERICCODEC_SamplingRateSet(myGENERICCODECHandle, 48000); _//Sets 48000 media sampling rate_C
void DRV_GENERICCODEC_SamplingRateSet(DRV_HANDLE handle, uint32_t samplingRate);