1.1.3.6.11 DRV_GENERICCODEC_VolumeGet Function
uint8_t DRV_GENERICCODEC_VolumeGet(DRV_HANDLE handle, DRV_GENERICCODEC_CHANNEL channel)Summary
This function gets the volume for Generic Codec.
Description
This functions gets the current volume programmed to the Generic Codec.
Preconditions
The DRV_GENERICCODEC_Initialize routine must have been called for the specified Generic Codec driver instance.
DRV_GENERICCODEC_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| channel | argument indicating Left or Right or Both channel volume to be modified |
Returns
None.
Remarks
None.
Example
_// myAppObj is an application specific object._ MY_APP_OBJ myAppObj; uint8_t volume; _// myGENERICCODECHandle is the handle returned // by the DRV_GENERICCODEC_Open function._ volume = DRV_GENERICCODEC_VolumeGet(myGENERICCODECHandle, DRV_GENERICCODEC_CHANNEL_LEFT);
C
uint8_t DRV_GENERICCODEC_VolumeGet(DRV_HANDLE handle, DRV_GENERICCODEC_CHANNEL channel);