4 Revision History
The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.
| Revision | Date | Description |
|---|---|---|
| A | 04/2024 | The following is the summary of changes made in revision A:
|
| 1.4 | 07/2016 | Updated text for errata item 2.19 The I/Os State during Programming is Changed from Z to Weak Pull-Up. |
| 1.3 | 04/2016 | Added errata items 2.20 For S (Security) Grade Devices, User Must Not Enable Write Protection for Protected 4 K Regions, Also Known as Special Sectors in the eNVM and 2.21 Users Must Not Set Page Lock in eNVM0 for the 060 Device and eNVM1 for 090/150 Devices. |
| 1.2 | 12/2015 | The following is the summary of changes made in revision 1.2:
|
| 1.1 | 08/2015 | Updated M2GL060 Revision from ES to Rev 0. |
| 1.0 | 06/2015 | The following is the summary of changes made in revision 1.0:
|