4.3.1 Delay
The Delay functionality is used by the ATWINC15x0 driver for synchronizing with ATWINC15x0 modules.
- Create
delay.canddelay.hfiles under the “source files” of the project. - Copy the following to the
delay.cfile:#ifndef DELAY_H #define DELAY_H #ifdef __cplusplus extern "C" { #endif // 1ms Count = 1ms / (1/((FOSC/2)/TMR Prescaler)) #define DELAY_1MS_COUNT 16 // Given FOSC/2 = 4MHz, TMR //Prescaler = 256: // TMR Period = 64us // 1ms / 64us = 15.6 => 16 /* * Timer control functions for the delay function * Set these values to the MCC generated functions for the TMR peripheral used for the delay. */ #define DELAY_TMR TMR1 #define DELAY_TMR_START() TMR1_Start() #define DELAY_TMR_STOP() TMR1_Stop() #define DELAY_TMR_PER_SET(period) TMR1_Period16BitSet(period) #define DELAY_TMR_COUNT_SET(count) TMR1_Counter16BitSet(count) void delay_timer_callback (); void delay_ms(); #ifdef __cplusplus } #endif - Copy the following to the
delay.hfile:#include <stdio.h> #include "mcc_generated_files/mcc.h" #include "delay.h" static bool delay_timer_expired = false; void delay_timer_callback (void) { delay_timer_expired = true; } void delay_ms(uint16_t ms) { DELAY_TMR_STOP(); DELAY_TMR_PER_SET ( (uint16_t)(ms * DELAY_1MS_COUNT) ); DELAY_TMR_COUNT_SET ( 0 ); delay_timer_expired = false; DELAY_TMR_START(); while (!delay_timer_expired) ; }