3.1.4.2 Start RX with MAC Filter Selection
The following table provides the command syntax for RX test with MAC filter selection.
| Command Syntax | MCHPRT X Y Z A | |||||
|---|---|---|---|---|---|---|
| X | X refers to RX mode:
| |||||
| Y | Y refers to TX channel: 1 to 14
| |||||
| Z | In Source MAC address In | |||||
| A | In | |||||
| Example |
MCHPRT 2_SA_Self_DA 1 112233445566 665544332211 RX with Source MAC filter: 112233445566 and DA MAC filter and Self MAC address: 665544332211 in Channel 1 Start with reset the count MCHPRT 2_SA_DA 12 112233445566 RX with Source MAC filter: 112233445566 in Channel 12 Start with reset the count MCHPRT 2_Self_DA 13 665544332211 RX with DA MAC filter and Self MAC address: 665544332211 in Channel 13 Start with reset the count | |||||
The following figure shows the example of RX with Source MAC filter: 112233445566 and DA MAC filter and Self MAC address: 665544332211 in Channel 1 Start with reset the count.

The following figure shows the example of RX with Source MAC filter: 112233445566 in Channel 12 Start with reset the count.

The following figure shows the example of RX with DA MAC filter and Self MAC address: 665544332211 in Channel 13 Start with reset the count.