5.2.1 HCI TX
Perform the following steps for TX.
- After successful initialization, select the TX tab to change to TX HCI command.
- Select the Channel.
- Select the Length.
- Select the Payload.
- Then the HCI command is shown in the TX command box.
- Click TX Start to send the TX HCI command.
Figure 5-5. Start TX 
- The sent and received HCI command is
shown in the log. Yellow represents the sent command [Hex] and Green represents the
received command [Hex].
Figure 5-6. Sent/Received HCI Command 
- Click TX Stop to send TX stop command.
Figure 5-7. Stop TX