24.5.2.5 Write Access Protection Management Errors
Only word-wise writes to the WRCTRL register effectively changes the access protection. Other types of accesses have no effect and cause a PAC write access error. This error is reported in the INTFLAGA.PAC bit.
PAC also offers an additional safety feature for correct program execution with an interrupt generated on double write clear protection or double write set protection. If a peripheral is write protected and a subsequent set protection operation is detected, the PAC returns an error and does so similarly for a double clear protection operation.
In addition, an error is generated when writing a set and lock protection to a write-protected peripheral or when a write access is done to a locked set protection. This can be used to ensure that the application follows the intended program flow by always following a write protect with an unprotect. However, in applications where a write-protected peripheral is used in several contexts, for example, interrupt, care must be taken so that either the interrupt cannot happen while the main application or other interrupt levels manipulate the write protection status or when the interrupt handler needs to unprotect the peripheral based on the current protection status by reading the STATUS register.
The errors generated while accessing the PAC module registers (for example, key error, double protect error and so on) set the INTFLAGA.PAC flag.