32.6.3.3 IrDA Modulation and Demodulation
Transmission and reception can be encoded IrDA compliant up to 115.2 kbps. IrDA modulation and demodulation work in the following configuration:
- IrDA encoding enabled (CTRLB.ENC = 1)
- Asynchronous mode (CTRLA.CMODE = 0)
- 16x sample rate (CTRLA.SAMPR[0] = 0)
During transmission, each low bit is transmitted as a high pulse. The pulse width is 3/16 of the baud rate period, as illustrated in the following figure.
- The first is to synchronize the incoming data to the IrDA baud rate counter. Synchronization is performed at the start of each zero pulse.
- The second main function is to decode incoming RX data. If a pulse width meets the minimum length set by configuration (RXPL.RXPL), it is accepted. When the baud rate counter reaches its middle value (1/2 bit length), it is transferred to the receiver.
- During transmission, a ‘
0’ bit is transmitted as a ‘1’ pulse - During reception, an accepted ‘
0’ pulse is received as a ‘0’ bit
Example: The following figure illustrates reception where RXPL.RXPL is set to 19. This indicates that the pulse width must be at least 20 SE clock cycles. When using BAUD = 0xE666 or 160 SE cycles per bit, this corresponds to 2/16 baud clock as minimum pulse width required. In this case, the first bit is accepted as a ‘0’, the second bit is a ‘1’ and the third bit is also a ‘1’. A low pulse is rejected because it does not meet the minimum requirement of 2/16 baud clock.