4 Initialization Example
This chapter aims to explain the different steps required during the initialization phase of the system. After powering up the PL360 device, a set of initialization sequences must be executed in the correct order for the proper operation of the PL360 device.
The steps are the following:
- Init controller descriptor
- Set controller callbacks
- Enable controller
- PL360 event handling
CAUTION: Failure to complete any of
the these initialization steps will result in failure in the PL360 Host Controller
startup.