1 PL360 Host Controller Architecture
The PL360 Host Controller is a C source code component which provides the host MCU application access to the API of the Power Line Communications PHY layer running in the PL360 device. Figure 1-1 shows the architecture of the software which runs on the host MCU. The components of the PL360 Host Controller are described in the following subsections.