5 Configuration
The PL360 Host controller is configured in the conf_atpl360.h file, which is described in Configure Application.
The PL360 firmware has a set of configurable parameters that control its behavior. These parameters are described in PIB Objects Specification and Access (G3) and PIB Objects Specification and Access (PRIME). In the applications provided by Microchip, there are examples of configuration and use of some of these parameters. In particular, some parameters need to be configured according to the PLC device used and/or the hardware design, as described in Zero-Crossing Configuration and Transmission Coupling Configuration.