39.8.4 SMC Mode Register
This register can only be written if the WPEN bit is cleared in the SMC Write Protection Mode Register. The user must confirm the SMC configuration by writing any one of the SMC MODE registers.
Symbol | Description | Symbol | Description | Symbol | Description |
---|---|---|---|---|---|
R | Readable bit | HC | Cleared by Hardware | (Grey cell) | Unimplemented |
W | Writable bit | HS | Set by Hardware | X | Bit is unknown at Reset |
K | Write to clear | S | Software settable bit | — | — |
Name: | MODE |
Offset: | 0x0C + n*0x04 [n=0..3] |
Reset: | 0x00 |
Property: | Read/Write |
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
PS[1:0] | PMEN | ||||||||
Access | R/W | R/W | R/W | ||||||
Reset | 0 | 0 | 0 |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
TDF MODE | TDF CYCLES[3:0] | ||||||||
Access | R/W | R/W | R/W | R/W | R/W | ||||
Reset | 0 | 0 | 0 | 0 | 0 |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
DBW | BAT | ||||||||
Access | R/W | R/W | |||||||
Reset | 0 | 0 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
EXNW MODE[1:0] | WRITE MODE | READ MODE | |||||||
Access | R/W | R/W | R/W | R/W | |||||
Reset | 0 | 0 | 0 | 0 |
Bits 29:28 – PS[1:0] Page Size
If page mode is enabled, this field indicates the size of the page in bytes.
Value | Name | Description |
---|---|---|
o | 4 BYTE | 4-byte page |
1 | 8 BYTE | 8-byte page |
2 | 16 BYTE | 16-byte page |
3 | 32 BYTE | 32-byte page |
Bit 24 – PMEN Page Mode Enabled
Value | Description |
---|---|
0 | Standard read is applied. |
1 | Asynchronous burst read in page mode is applied on the corresponding chip select. |
Bit 20 – TDF MODE TDF, Data Float Time, Optimization
Value | Description |
---|---|
0 | TDF optimization disabled-the number of TDF wait states is inserted before the next access begins. |
1 | TDF optimization enabled-the number of TDF wait states is optimized using the setup period of the next read/write access. |
Bits 19:16 – TDF CYCLES[3:0] Data Float Time
This field gives the integer number of clock cycles required by the external device to release the data after the rising edge of the read controlling signal. The SMC always provide one full cycle of bus turnaround after the TDF CYCLES period. The external bus cannot be used by another chip select during TDF CYCLES + 1 cycles. From 0 up to 15 TDF CYCLES can be set.
Bit 12 – DBW Data Bus Width
Value | Name | Description |
---|---|---|
o | 8 BIT | 8-bit Data Bus |
1 | 16 BIT | 16-bit Data Bus |
2 | 32 BIT | 32-but Data Bus |
3 | - | Reserved |
Bit 8 – BAT Byte Access Type
This field is used only if DBW defines a 16-bit data bus.
Value | Name | Description |
---|---|---|
o | BYTE SELECT | Byte select access type:
|
1 | BYTE WRITE | Byte write access type:
|
Bits 5:4 – EXNW MODE[1:0] NWAIT Mode
The NWAIT signal is used to extend the current read or write signal. It is only taken into account during the pulse phase of the read and write controlling signal. When the use of NWAIT is enabled, at least one cycle hold duration must be programmed for the read and write controlling signal.
Value | Name | Description |
---|---|---|
o | DISABLED | Disabled-The NWAIT input signal is ignored on the corresponding chip select. |
1 | Reserved | |
2 | FROZEN | Frozen Mode-If asserted, the NWAIT signal freezes the current read or write cycle. After deassertion, the read/write cycle is resumed from the point where it was stopped. |
3 | READY | Ready Mode-The NWAIT signal indicates the availability of the external device at the end of the pulse of the controlling read or write signal, to complete the access. If high, the access normally completes. If low, the access is extended until NWAIT returns high. |
Bit 1 – WRITE MODE Write Mode
Value | Name | Description |
---|---|---|
0 | NCS_CTRL | Write operation controlled by NCS signal—If TDF optimization is enabled (TDF_MODE = 1), TDF wait states will be inserted after the setup of NCS. |
1 | NWE_CTRL | Write operation controlled by NWE signal—If TDF optimization is enabled (TDF_MODE = 1), TDF wait states will be inserted after the setup of NWE. |
Bit 0 – READ MODE Read Mode
Value | Name | Description |
---|---|---|
0 | NCS_CTRL | Read operation controlled by NCS signal
|
1 | NRD_CTRL | Read operation controlled by NRD signal
|