3.1.2.3 BLE Extended Advertisements
Getting Started with Peripheral Building Blocks
Introduction
This document will help users enable Extended Advertisements (1M, 2M, coded PHY -- 125kbps) on WBZ451 Curiosity Board. This example (ext_adv) enables users to send application data using extended advertisements. Extended Advertisements are used to send more data than the legacy advertisements allow and allow long range functionality when using Coded PHY. Use of Extended Advertisements also enables the users to select between different PHYs (1M, 2M and LE Coded) which are not permitted when using legacy advertisements. In BLE a peripheral or broadcaster always starts with advertisements. Advertisement packets enable a central or observer to discover a peripheral or broadcaster.
Extended Advertisements implemented in this example can be used for sending more data (2M PHY) or do range tests (Coded PHY). For testing these features a scanner Application can be used which is configured to scan the extended advertisement packets.
To save power, low power mode can be enabled. If conditions are met then WBZ451 will enter into sleep mode. The following sections discuss it in details.
Users can run the precompiled Application Example hex file provided with this example on the WBZ451 Curiosity Board and go through the steps involved in developing this Application application from the scratch
These examples each build on top on one and other. We strongly recommend that you follow the examples in order, to learn the basics concepts before progressing to the more advanced topics.
Recommended Reading
Hardware Requirement
Tool | Qty |
---|---|
WBZ451 Curiosity Board | 1 (2 if testing with a scanner) |
Micro USB cable | 1 |
SDK Setup
Software Requirement
Smartphone App
None
Programming the Precompiled Hex File or Application Example
Programming the hex file using MPLABX IPE
-
Precompiled Hex file is located in
"<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\ext_adv\hex"
folder -
For more details on the steps, go to Programming A Device .Note: Ensure to choose the correct Device and Tool information.
Programming the Application using MPLABX IDE
-
Follow steps mentioned in of Running a Precompiled Example document
-
Open and program the Application Example "ext_adv.x" located in
"<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\ext_adv\firmware
" using MPLABX IDE
For more details on how to find the Harmony Content Path, refer to Installing the MCC Plugin
Demo Description
This Application Example enables users to transmit Extended Advertisements @ Coded PHY data rate of 125 Kbps. PDU types of ADV_EXT_IND and ADV_AUX_IND will be transmitted. Application data ("Microchip") is transmitted in Auxiliary packets (ADV_AUX_IND). ADV_EXT_IND carries the Auxiliary Packet Information (ADV_AUX_IND) for scanner to collect the data.
Demo will print "Ext Adv Enabled" information indicating the successful start of Coded PHY Advertisements on a terminal emulator like TeraTerm @ (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none). Coded PHY Advertisements are configured to be sent every 2 secs.
BLE Extended Advertisements (125 kbps, 500 kbps)cannot be scanned using a smartphone app. This could be due to support of only legacy advertisements on the smartphone or disabled extended adv API's in smartphone app.
Testing
Users can use another WBZ451 Curiosity Board configured as BLE Scan Ext Adv
This section assumes that a user has already programmed the ext_adv and scan_ext_adv application on 2 WBZ451 Curiosity Boards.
Board1: WBZ451 Curiosity Board with Ext Adv Programmed
Board2: WBZ451 Curiosity Board with Scan Ext Adv Programmed
Board1: Open TeraTerm @ (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none). Reset the board. Upon reset, "Ext Adv Enable" message is displayed on the TeraTerm.
Board2: Open TeraTerm @ (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none). Reset the board. Upon reset, "ExtAdv Scan Enable Success" message is displayed on the TeraTerm. "Microchip" message will be displayed as soon the WBZ451 module performs an extended advertisement scan.
Current Consumption Measurement
Users of this package should go through the known issues document and understand the limitations if any with the current low power mode implementation.
Developing this Application from Scratch using MPLAB Code Configurator
- Setup Harmony framework. EA release package has all the neccessary component and should be downloaded individually from the link provided in the package. It is recommended to create framework in the root directory. The framework looks like:
Create a new MCC Harmony Project. For more details on creating a new MCC Harmony Project, refer to 2.5 Creating a New MCC Harmony Project .
-
Drag and drop BLE_Stack in the project graph and select Yes to all pop ups. Drag and Drop SERCOM0 from Peripherals into project graph for UART messages. Project Graph will look like
-
Enable Low Power
– Enable Low power mode by selecting Low Power Enable in BLE_Stack Configuration. Select Yes to all pop upsClick on Window->MCC->Harmony->Clock Configuration
Advertisement Configuration
- Select BLE_Stack component in project graph and make modifications as shown below
Configuring UART
For more details on UART Configuration, refer to UART Hello World
Generating a Code
For more details on code generation, refer to on MPLAB Code Configurator(MCC) Code Generation.
Files and Routines Automatically Generated by the MCC
Source Files | Usage |
---|---|
app.c |
Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble\ app_ble.c |
Source Code for the BLE stack related component configurations, code related to function calls from app.c |
app_ble\app_ble_handler.c |
All GAP, GATT, SMP and L2CAP Event handlers |
app_user_edits.c |
User Code Change instruction |
Header Files
-
ble_gap.h
: This header file contains BLE GAP functions and is automatically included in theapp.c
file
Function Calls
MCC generates and adds the code to initialize the BLE Stack GAP, GATT, L2CAP and SMP in APP_BleStackInit() function
-
APP_BleStackInit() is the API that will be called inside the Applications Initial State -- APP_STATE_INIT in app.c
-
RTC_Timer32Start() defined in plib_rtc_timer.c. It call to start RTC Timer clock to facilitate low Power mode.
User Application Development
Include
-
definitions.h
in all the files where UART will be used to print debug informationNote:definitions.h
is not specific to just UART peripheral, instead it should be included in all application source files where peripheral functionality will be exercised
-
User action is required as mentioned in User Action
Start Ext Advertisement
-
BLE_GAP_SetExtAdvEnable(true, 0x01, &extAdvEnableParam);
Users can exercise various other BLE Advertisement functionalities by using BLE Stack API