This document will help users enable advertisements and connection on the WBZ451 Curiosity board using the MPLAB Code
Configurator(MCC). The peripheral device will be the WBZ451 Curiosity board and the central device can either be a smartphone
with a Light Blue app or another WBZ451 Curiosity board.
BLE Advertising is broadcasting small packets to peer devices. In BLE, a peripheral
device always starts with advertisements. Advertisement packets enable a central or
observer to discover and connect to a peripheral.
Users can choose to just run the precompiled Application Example hex file on the WBZ451 Curiosity board and experience the demo or can go
through the steps involved in developing this application from scratch.
It is recommended to follow the examples in order, by learning the basic concepts
first and then progressing to the more advanced topics.
Programming the Precompiled Hex File
or Application Example
Programming the .hex File using
MPLAB X IPE
Import and program the
Precompiled .hex file: <Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\peripheral_conn\hex\peripheral_conn.X.production.signed.hex
Open and program the application:
“<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\peripheral_conn\firmware\peripheral_conn.X
This application enables users to transmit Connectable and Scannable Undirected BLE
Advertisements. On reset, demo will print "Advertising" on a terminal emulator like
Tera Term which denotes the start of advertisements. The central device scanning
these advertisements can then issue a connection request unto the Curiosity board.
Upon connection, "Connected" is printed on the terminal window.
Testing
Using a micro USB cable, connect
the Debug USB on the Curiosity board to a PC
Program the precompiled hex file or application example as mentioned
Open Tera Term and set the
“Serial Port” to USB Serial Device and “Speed” to 115200.
For more details
on how to set the “Serial Port” and “Speed”, refer to COM Port Setup
Press the Reset Switch on the
Curiosity board. "Advertising" should be displayed in Tera Term.
Launch the Light Blue mobile app
to scan for Advertisements. The device name "Microchip" will appear then press
Connect. After a successful connection, you can view the advertisement data and
see “Connected” displayed in Tera Term.
Developing the Application from
Scratch using MCC
This section explains the steps required by a user to develop this application
example from scratch using the MPLAB Code Configurator
Note: It is recommended that new users of the MPLAB Code
Configurator to go through this overview
To setup the basic components and
configuration required to develop this application, import component
configuration: <Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\peripheral_conn\firmware\peripheral_conn.X\peripheral_conn.mc3
Note: Import and export functionality of Harmony
component configuration will help users to start from a known working
setup of MCC configuration
To accept dependencies or
satisfiers, select "Yes"
Verify if the project graph
window has all the expected configuration. as illustrated in the following
figure:
Figure 3-103. Project Graph
Verifying Advertisement and
Connection Configuration
Select BLE Stack component in project
graph, to open component configuration and configure as illustrated in the
following figure.
Figure 3-104. BLE Stack
Configuration
Note: If users cannot see the Configuration Options panel in the right-hand
side of the MPLAB X IDE, it might be minimized. Hover the cursor towards
the Configuration Options side tab and click the “dot” on the top
right-hand corner to pin it (see the following figure)Figure 3-105. Configuration Panel
Files and Routines Automatically
Generated by the MCC
After generating the program source from MCC interface by clicking Generate Code, the
BLE configuration source and header files can be found in the following project
directoriesFigure 3-106. Project File
The OSAL, RF System and BLE System
initialization routine executed during program initialization can be found in the
project file. This initialization routine is automatically generated by the MCC.
Figure 3-107. initialization.c
The BLE stack initialization routine executed during Application Initialization can
be found in project files. This initialization routine is automatically generated by
the MCC. This call initializes and configures the GAP, GATT, SMP, L2CAP and BLE
middleware layers.
Figure 3-108. app_ble.c
Here are also the autogenerated Advertisement Data (AD) structures and types as
referenceFigure 3-109. AD Structures and Types
Table 3-15. Source Files
Source Files
Usage
app.c
Application State machine, includes calls for Initialization of
all BLE stack (GAP,GATT, SMP, L2CAP) related component
configurations
app_ble\app_ble.c
Source Code for the BLE stack related component configurations,
code related to function calls from app.c
app_ble\app_ble_handler.c
All GAP, GATT, SMP and L2CAP Event handlers
Note:app.c is autogenerated and has a state machine based application
code. Users can use this template to develop their own application.
Header Files
ble_gap.h
contains BLE GAP functions and is automatically included in
app.c file.
Function Calls
MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and
L2CAP in APP_BleStackInit()
APP_BleStackInit() is the API that will be called inside the Applications
Initial State APP_STATE_INIT in app.c
definitions.h must be included in all the files where UART
will be used to print debug information
Note: definitions.h is not specific to just UART
but instead it must be included in all application source files where any peripheral
functionality will be exercised
All the possible GAP, GATT, SMP
and L2CAP Event handlers are available in file
app_ble_handler.c. Users can implement their own
application code to denote Connection State here.Figure 3-112. app_ble_handler.c
Users can exercise various other BLE advertisement functionalities by using the BLE Stack APIs