3.1.2.6 BLE Transparent UART
Getting Started with Peripheral Building Blocks
BLE Connection -> BLE Transparent UART
Introduction
This section helps users to create a peripheral device and send/receive characters between two connected BLE devices over Microchip proprietary Transparent UART Profile. Peripheral device will be the WBZ451 Curiosity board and central device can either be a Smart phone with Light Blue app or another WBZ451 Curiosity board.
Users can choose to run the precompiled application example .hex
file on
the WBZ451 Curiosity board and experience the demo or go through
the steps involved in developing this application from scratch.
Recommendation is to follow the examples in order, by learning the basic concepts first and then progressing to the more advanced topics.
Recommended Reading
Hardware Requirement
Tool | Qty |
---|---|
WBZ451 Curiosity Board | 1 |
Micro USB cable | 1 |
Android/iOS Smart phone | 1 |
SDK Setup
Software Requirement
Smart phone App
-
Light Blue iOS/Android app available in stores
Programming the Precompiled Hex File or Application Example
Programming the .hex
File using MPLAB X IPE
- Import and program the precompiled
.hex
file is located in"<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\Peripheral\profiles_services\peripheral_trp_uart\hex\peripheral_trp_uart.hex"
folder - For more details on the steps, go to
Programming a DeviceNote: Users must choose the correct device and tool information
Programming the Application using MPLAB X IDE
- Follow steps mentioned in the Running a Precompiled Example section.
- Open and program the application example
"
peripheral_trp_uart.X
" located in "<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\profiles_services\peripheral_trp_uart\firmware\peripheral_trp_uart.X"
using MPLAB X IDEFor more details on finding the Harmony content path, refer to Installing the MCC Plugin
Demo Description
This application enables users to send data back and forth over UART between two connected BLE devices. On Reset, demo application prints “Advertising” which denotes the start of advertisements and then “Connected” when connection is established. Application data to be sent to the connected central device (smart phone or another WBZ451 Curiosity board) is entered in a terminal emulator like Tera Term.
Testing
- Using a Micro USB cable, connect the Debug USB on the Curiosity board to a PC. The Active LED turns Green once connected to the PC.
- Program the precompiled hex file or application example as mentioned.
- Open TeraTerm and configure as mentioned
below:Terminal Settings
- Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
- Parity – None
- Data Bits – 8
- Stop Bits – 1
- Flow Control – None
For more details on how to set the “Serial Port” and “Speed”, refer to COM Port Setup.
- Press the Reset Switch on the Curiosity board.
- Launch the Light Blue mobile app and search for the device name “pic32cx-bz/Microchip” and press Connect.
- To receive data from the WBZ451 Curiosity board (peripheral device) to the mobile app (central device), select “UUID: 49535343-1E4D-4BD9-BA61-23C647249616” then select Subscribe.
- Change the Data format to UTF-8 String in
the Light Blue mobile app then enter "test" on Tera Term. The same data must be displayed
in the app.Note: User may not be able to see “test” on the Tera Term as user types.
- To send data from the mobile app (central device) to the WBZ451 Curiosity board (peripheral device), select “UUID: 49535343-8841-43F4-A8D4-ECBE34729BB3”.
- Change the Data format to UTF-8
String then enter “trp uart” and click Write. The same data must be
displayed in Tera Term (see the following figure).Note: Users can use another WBZ451 Curiosity board configured as BLE Transparent UART (central) instead of using a mobile app.
Developing the Application from Scratch using MCC
- Create a new MCC Harmony Project. For more details, refer to Creating a New MCC Harmony Project.
- Import component configuration – This
step helps users setup the basic components and configuration required to develop this
application. The imported file is of format
.mc3
and is located in the path<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\building_blocks\peripheral\profiles_services\peripheral_trp_uart\firmware\peripheral_trp_uart.X.
For more details on importing the component configuration , refer to Importing Existing App Example Configuration .
Note: Import and export functionality of Harmony component configuration will help users to start from a known working setup of MCC configuration. - Accept dependencies or satisfiers, select Yes.
- Verify if the project graph window has
all the expected configuration. as illustrated in the following figure:Note: Ensure that the macro
configUSE_TICKLESS_IDLE
is set to0
. The macro is available inFreeRTOSConfig.h
file#define configUSE_TICKLESS_IDLE 0
Verifying Advertisement,Connection and Transparent UART Profile Configuration
-
Select BLE Stack component in project graph, to open component configuration and configure as illustrated in the following figure.
Note: If users cannot see the Configuration Options panel in the right-hand side of the MPLAB X IDE, it might be minimized. Hover the cursor towards the Configuration Options side tab and click the “dot” on the top right-hand corner to pin it (see the following figure).. - Select Transparent Profile component in project graph, to open component configuration and configure as illustrated in the following figure.
Generating a Code
For more details on code generation, refer to the MPLAB Code Configurator(MCC) Code Generation section.
Files and Routines Automatically Generated by the MCC
Source Files | Usage |
---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble\app_ble.c | Source Code for the BLE stack related component configurations, code related to function
calls from app.c |
app_ble\app_ble_handler.c | All GAP, GATT, SMP and L2CAP Event handlers |
app_ble\app_trsps_handler.c | All Transparent UART Server related Event handlers |
ble_trsps.c | All Transparent Server Functions for user application |
app.c
is autogenerated and has a state machine
based application code. Users can use this template to develop their own application.Header Files
ble_gap.h
: Contains BLE GAP functions and is automatically included in theapp.c
file.ble_trsps.h
: is associated with APIs and structures related to BLE Transparent Client functions for application user.
Function Calls
- MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and L2CAP in
APP_BleStackInit()
function. APP_BleStackInit()
is the API that will be called inside the Applications Initial State --APP_STATE_INIT
inapp.c
.
User Application Development
Include
- User action is required as mentioned User Action.
ble_trsps.h
inapp.c
, BLE Transparent UART Server related APIs.osal/osal_freertos_extend.h
inapp_trsps_handler.c
, OSAL related APIs are available here.definitions.h
must be included in all the files where UART will be used to print debug information.Note:definitions.h
is not specific to just UART but instead must be included in all the application source files where any peripheral functionality will be exercised.
Set Public Device Address in app_ble.c
BLE_GAP_SetDeviceAddr(&devAddr);
BLE_GAP_Addr_T devAddr;
devAddr.addrType = BLE_GAP_ADDR_TYPE_PUBLIC;
devAddr.addr[0] = 0xA1;
devAddr.addr[1] = 0xA2;
devAddr.addr[2] = 0xA3;
devAddr.addr[3] = 0xA4;
devAddr.addr[4] = 0xA5;
devAddr.addr[5] = 0xA6;
// Configure device address
BLE_GAP_SetDeviceAddr(&devAddr);
Starting Advertisement
BLE_GAP_SetAdvEnable(0x01, 0x00);
Connected and Disconnected Events
In
app_ble_handler.c
,BLE_GAP_EVT_CONNECTED
event will be generated when a BLE connection is completed
Connection Handler
- Connection handle associated with the peer peripheral device needs to be saved for data exchange after a BLE connection
p_event->eventField.evtConnect.connHandle
has this information
Transmit Data
- Add “
APP_MSG_UART_C
” to the generatedAPP_MsgId_T
BLE_TRSPS_SendData(conn_hdl , 1, &data);
is the API to be used for sending data to the central device.Note: The precompiled application example uses a UART callback to initiate the data transmission upon receiving a character in UART.-
Example for transmitting over UART using the
BLE_TRSPS_SendData()
API
uint16_t conn_hdl;// connection handle info captured @BLE_GAP_EVT_CONNECTED event
uint16_t ret;
uint8_t uart_data;
void uart_cb(SERCOM_USART_EVENT event, uintptr_t context)
{
APP_Msg_T appMsg;
// If RX data from UART reached threshold (previously set to 1)
if( event == SERCOM_USART_EVENT_READ_THRESHOLD_REACHED )
{
// Read 1 byte data from UART
SERCOM0_USART_Read(&uart_data, 1);
appMsg.msgId = APP_MSG_UART_CB;
OSAL_QUEUE_Send(&appData.appQueue, &appMsg, 0);
}
}
void APP_UartCBHandler()
{
// Send the data from UART to connected device through Transparent service
BLE_TRSPS_SendData(conn_hdl, 1, &uart_data);
}
// Register call back when data is available on UART for Peripheral Device to send
// Enable UART Read
SERCOM0_USART_ReadNotificationEnable(true, true);
// Set UART RX notification threshold to be 1
SERCOM0_USART_ReadThresholdSet(1);
// Register the UART RX callback function
SERCOM0_USART_ReadCallbackRegister(uart_cb, (uintptr_t)NULL);
else if(p_appMsg->msgId==APP_MSG_BLE_STACK_LOG)
{
// Pass BLE LOG Event Message to User Application for handling
APP_BleStackLogHandler((BT_SYS_LogEvent_T *)p_appMsg->msgData);
}
else if(p_appMsg->msgId==APP_MSG_UART_CB)
{
// Pass BLE UART Data transmission target BLE UART Device handling
APP_UartCBHandler();
}
Receive Data
BLE_TRSPS_EVT_RECEIVE_DATA
is the event generated when data is sent from the central device- Use the
BLE_TRSPS_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len);
API to extract the length of the application data received BLE_TRSPS_GetData(p_event->eventField.onReceiveData.connHandle, data);
API is used to retrieve the dataNote:BLE_TRSPS_Event_T p_event
structure stores the information about BLE transparent UART callback functions.- Example for printing the received data from the central device over UART
/* TODO: implement your application code.*/
uint16_t data_len;
uint8_t *data;
// Retrieve received data length
BLE_TRSPS_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len);
// Allocate memory according to data length
data = OSAL_Malloc(data_len);
if(data == NULL)
break;
// Retrieve received data
BLE_TRSPS_GetData(p_event->eventField.onReceiveData.connHandle, data);
// Output received data to UART
SERCOM0_USART_Write(data, data_len);
// Free memory
OSAL_Free(data);
Users can exercise various other BLE advertisement functionalities by using BLE Stack APIs.
Where to go from Here
- BLE Sensor App – this application utilizes the Transparent UART building block.