3 Component Tests
Acceptable Fault detection measures and considerations for some of the
individual components in Table 2-1, that are relevant to the
tinyAVR® 1-series, are described in this chapter.
Note: The single channel structure with a
functional test cannot be used if functional test is not listed under acceptable
measures for the components used in the appliance.