1.2 Prerequisites
(Ask a Question)Before you begin, ensure that the following components are in
place:
- Download and install Libero® SoC on the host PC from the following location: Libero SoC Installation link .
- Download the demo design files from www.microchip.com/en-us/application-notes/AN4682.
- Install the GUI application by running the
setup.exefile available in the design files folder:.At the end of the installation, you may be prompted to download and install the FPGA_GUI_Pack, if it is not already available on your system.
- Alternatively, you can manually download and install the Microchip FPGA_GUI_Pack.