12.4 Viewing Physical Device Error Counters
To view the physical device error counters for a hard drive or SSD, select the drive in the Enterprise View then, on the Storage Dashboard, click the Error Counters tab. The table below describes the error counters.
![](GUID-BF0CFEFD-6B79-47A1-B9BA-4708AB24A0B5-high.png)
Error Counter |
Description |
---|---|
Aborted Command |
Number of times a drive was failed due to aborted commands that could not be retried successfully. |
Bad Target Error |
Number of times that this drive did something that did not conform to the SCSI Bus Protocol. It will cause a reset of the SCSI bus that this drive is attached to. |
ECC Recovered Read Errors |
Number of ECC‑corrected read errors. |
Failed Read Recover |
Number of times a recover of another physical drive in the logical volume failed due to a hard read error from this drive. |
Failed Write Recover |
Number of times a recover of this physical drive failed due to an error occurring on this drive during a write operation. |
Format Error |
Number of times a Format command (used when remapping defects) failed. A failed remap operation may cause the controller to fail a drive. |
Hardware Error |
Number of times a drive returned a bad hardware status. The drive may be failed if retries do not work. |
Hard Read Error |
Number of unrecoverable read errors. |
Hard Write Error |
Number of unrecoverable write errors. |
Hot-Plug Count |
Number of times this drive was hot-plugged (removed) from a box. |
Media Failure |
Number of times a drive was failed due to unrecoverable media errors. |
Not Ready Error |
Number of times the drive was failed because it never became ready after the “spin up” command was issued. If retries or drive spin-ups fail, the drive will be failed. |
Other Timeouts |
Timeouts other than Data ReQuest Timeouts (DRQ). |
Predictive Failure |
Number of times that the drive returned a predictive failure error. |
Retry Recovered Read Error |
Number of retry‑recovered read errors. |
Retry Recovered Write Error |
Number of retry‑recovered write errors. |
SCSI Bus Fault |
Number of “bus faults”, which we define as SCSI bus parity errors, overrun/underrun conditions, etc. |
Service Hours |
Number of service hours since the last power cycle. |
Sectors Written |
Number of sectors written to media. |
Sectors Read |
Number of sectors read from the media. This value will include sectors read into the on-drive cache buffer only if the drive keeps track of this value. Otherwise, only sectors requested through the drive interface are counted. |