5.6.2 Modify Array
Add Drives
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device SED security status and SED qualification status:
SED Security Status |
SED Qualification Status |
---|---|
Locked |
Not Applicable |
Not Applicable |
Failed Locking Enabled |
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status.
Original Factory State (OFS) |
SED Ownership Status |
---|---|
False | Otherwise Owned |
False | MCHP Owned, Foreign |
False | Otherwise Owned, Foreign |
Add drives operation to an existing array will be blocked when the Array has the following status:
Array Status |
---|
One or more logical drives undergoing or failed SED qualification |
Has Logical Drive with Foreign SED |
When the Array status is OK, changing an existing drive(s) with SED drives of same type in the array is not allowed based on the physical device SED security status and SED qualification status:
SED Security Status |
SED Qualification Status |
---|---|
Locked |
Not Applicable |
Not Applicable |
Failed Locking Enabled |
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status:
Original Factory State (OFS) | SED Ownership Status |
---|---|
False | Otherwise Owned |
False | MCHP Owned, Foreign |
False | Otherwise Owned, Foreign |
Move drives operation on array will be blocked when the Array has the following status:
Array Status |
---|
One or more logical drives undergoing or failed SED qualification |
Has logical drive with foreign SED |
When the Array status is OK, changing existing drives of different type with SED drives of different type in the array is not allowed based on the following physical device SED security status and SED qualification status:
SED Security Status |
SED Qualification Status |
---|---|
Locked |
Not Applicable |
Not Applicable |
Failed Locking Enabled |
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status:
Original Factory State (OFS) | SED Ownership Status |
---|---|
False | Otherwise Owned |
False | MCHP Owned, Foreign |
False | Otherwise Owned, Foreign |
Change drive type operation on array will be blocked when the Array has the following status:
Array Status |
---|
One or more logical drives undergoing or failed SED qualification |
Has Logical Drive with Foreign SED |
When the Array status is “Has Failed Physical Device”, replacing failed drives with SED drives in the array is not allowed based on the following physical device SED security status and SED qualification status:
SED Security Status |
SED Qualification Status |
---|---|
Locked |
Not Applicable |
Not Applicable |
Failed Locking Enabled |
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status:
Original Factory State (OFS) | SED Ownership Status |
---|---|
False | Otherwise Owned |
False | MCHP Owned, Foreign |
False | Otherwise Owned, Foreign |
Modify Array ribbon icon should be disabled on the following Array status:
Array Status |
---|
Has Logical Drive with Foreign SED |