5.6.5 maxCache
On Existing Array
Create logical device operation on an existing array is blocked when the target Array has the following status:
Array Status |
---|
One or more logical drives undergoing or failed SED qualification |
Has Logical Drive with Foreign SED |
Create maxCache operation on existing cache array should be blocked when the target Array has the following status:
Cache Array SED Encryption Status | Logical Device SED Encryption Status |
---|---|
Encrypted=True | Encrypted=False |
Encrypted=False | Encrypted=True |
On New Array
The SED drives can be included in the new Array creation based on the following physical device SED security and SED qualification status.
SED Security Status | SED Qualification Status |
---|---|
Locked |
Not Applicable |
Not Applicable |
Failed Locking Enabled |
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status:
Original Factory State (OFS) | SED Ownership Status |
---|---|
False | Otherwise Owned |
False | MCHP Owned, Foreign |
False | Otherwise Owned, Foreign |