5.6.1 Create Logical Device

On Existing Array

Create logical device operation on an existing array will be blocked when the target Array has the following status:

Array Status Create Array Allowed/Not Allowed
One or more logical drives undergoing or failed SED qualification Creation not allowed

On New Array

The following table lists the physical device SED security status and SED qualification status, based on which the SED drives must be included in the new Array creation.

SED Security Status SED Qualification Status Create Array Allowed/Not Allowed
Locked

Not Applicable

Creation not allowed

Not Applicable

Failed Locking Enabled

Creation allowed

Not Applicable

Failed Range Length Set

Creation allowed