18.3 Monitoring maxView Resources in vSphere 7 HTML Client
For each maxView resource in your storage space─controller, logical device, physical device, and so on—you can view summary information about the resource (or "object") and view its related resources, such as the physical devices in a logical drive, the logical drives on a controller, or the controllers on a host.
For example, the following figure shows the added ESXi server.
![](GUID-E10B2EFD-DD23-4A90-9EC6-875900FDC2CC-high.png)
Click on the system IP address to navigate to the two tabs listed in the following table.
![](GUID-9249A67F-A617-4FB5-A2EC-5402C47AFAAC-high.png)
Tab |
Details |
---|---|
Getting Started |
Provide details on the ESXi server |
More Objects |
List the controller details |