13.2.1.1 What Do the Event Status Icons Mean?

maxView Storage Manager indicates event status with icons. This table lists the three categories, or types, of events based on severity.

Icon

Status

Examples

Information

The local system successfully connected to a remote system.

A logical drive was created.

A hot spare was deleted.

Warning

A logical drive is in a degraded state.

A disk drive is being rebuilt.

A controller is not responding to an enclosure.

Error

A controller has failed.

A logical drive has failed.

A disk drive or hot spare has failed.

An enclosure is overheating.

Multiple fans or power supplies within an enclosure have failed.

An enclosure is not responding.