4.2.3 Build DT- Overlay
By default, KERNEL_DIR in the Makefile is set to a
linux directory that would be under the parent directory in the
directory tree that is ../linux. Change it and provide the path to the
newly build kernel to this variable KERNEL_DIR. Our newly build zImage
and dtb file are available in this kernel.
This is needed because the DT Overlay repository uses the Device Tree Compiler (DTC) from the kernel source tree.
.itb) file using the following
commands:$ make sama5d3_xplained_dtbos
$ make sama5d3_xplained.itbThe process will generate sama5d3_xplained.itb file and is available in
the dt-overlay-at91 directory.