3.3.1 IO Editor—Signal Integrity
(Ask a Question)To access the Signal Integrity tab from IO Editor:
- Open Constraint Manager > Edit > Edit with I/O Editor.
Figure 3-2. IO Editor—XCVR View
- In the XCVR View [active] tab, select Signal Integrity View tab and the XCVR lane to edit signal integrity settings as shown in the following figure. Signal Integrity panel displays the default values from the initial PDC when XCVR is created by the Libero SoC software. If user modifies the default values in the Signal Integrity tab of the IO Editor, it writes in the PDC.