17.1.9.1.2 set_device
(Ask a Question)Description
Specify family name, die name, and speed grade.
set_device -family <family_name> -die <die_name> -speed <speed>
Arguments
Parameter | Type | Description |
---|---|---|
-family <family_name> | String | Specify the family name. Possible values are PolarFire®, PolarFire SoC. |
-die <die_name> | String | Specify the die name. |
-speed <speed> | String | Specify the device speed grade. Possible values are STD or -1. |
Return Type | Description |
---|---|
0 | Command succeeded. |
1 | Command failed. There is an error. You can observe the error message in the console. |
List of Errors
Error Code | Error Message | Description |
---|---|---|
ERR0023 | Required parameter—die is missing | The die option is mandatory and must be specified. |
ERR0005 | Unknown die 'MPF30' | The value of -die option is not correct. See the possible list of values in option's description. |
ERR0023 | Parameter—die is missing value | The die option is specified without value. |
ERR0023 | Required parameter—family is missing | The family option is mandatory and must be specified. |
ERR0004 | Unknown family 'PolarFire®' | The family option is not correct. See the possible list of values in option's description. |
ERR0023 | Parameter—family is missing value | The family option is specified without value. |
ERR0023 | Required parameter—speed is missing | The speed option is mandatory and must be specified. |
ERR0007 | Unknown speed '<speed>' | The speed option is not correct. See the possible list of values in option's description. |
ERR0023 | Parameter—speed is missing value | The speed option is specified without value. |
Example
set_device -family {PolarFire} -die {MPF300T_ES} -speed -1
set_device -family SmartFusion 2 -die M2S090T -speed -1