21.10.16 set_manufacturer

Description

This command specifies the manufacturer for the SPI Flash device.

set_manufacturer {MICRON | SPANSION | Macronix | Winbond }

Arguments

ParameterTypeDescription
NonestringThe value for the set_manufacturer command must be one of the following:
  • MICRON
  • SPANSION
  • Macronix
  • Winbond
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneNone

Supported Families

PolarFire®
PolarFire SoC

Example

This example sets the manufacturer {MICRON}.

set_manufacturer {MICRON}