21.10.15 set_auto_update_mode
(Ask a Question)Description
This Tcl command enables or disables auto update. This command is added to the spiflash.cfg file that is given as the parameter to the configure_spiflash command.
set_auto_update_mode {0|1}
Arguments
Parameter | Type | Description |
---|---|---|
None | boolean | If set_auto_update_mode is 0, auto update is disabled. If set_auto_update_mode is 1, auto update is enabled. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | None |
Supported Families
PolarFire® |
PolarFire SoC |
Example
This example sets auto update disabled.
set_auto_update_mode {0}