2.1 Latest Release
(Ask a Question)View/Download the latest Libero SoC Design Suite documentation
2.1.1 Download Libero SoC Design Suite Help Documentation
(Ask a Question)Click here to download a copy of the latest
            Libero SoC Design Suite Help documentation (in HTML file format) for offline reference.
            Extract the contents of the .zip archive and open the
                index.html file in a web browser of your choice.
2.1.2 PDF Document Catalog v2025.1
(Ask a Question)Libero documentation is updated frequently. As a result, the PDF documents released with the Libero SoC Design Suite might not be the current version. You can use the following table to access the latest version of a Libero SoC document on the Microchip website. Click a document title to view the PDF file (requires an Internet connection). You will need a PDF reader to open the PDF files. Alternatively, you can open PDF files in most modern browsers, though they may lack some features.
| Document Title | Description | 
|---|---|
| Design Flow User Guide for SmartFusion2, IGLOO2, and RTG4 | Explains how to use the Libero SoC Project Manager with PolarFire, SmartFusion2, IGLOO2, and RTG4 devices. | 
| PolarFire Block Flow User Guide | Describes the Block Flow, that enables you to use design blocks (components) as building blocks for your top-level designs. | 
| PolarFire Custom Flow User Guide | Describes the Custom Flow for PolarFire® and PolarFire SoC family of devices, a process to integrate Libero as a part of the larger FPGA design flow | 
| Custom Flow User Guide | Describes the Custom Flow, a process to integrate Libero as a part of the larger FPGA design flow. | 
| Chip Planner User Guide | Describes how to use Chip Planner for design floorplanning. | 
| I/O Editor User Guide | Explains how to use the I/O Editor to edit constraints. | 
| Netlist Viewer User Guide | 
                             Describes Netlist Viewer invoked stand-alone from the Libero Design Flow window and available in pre-synthesis, post-synthesis, and post-layout phase of design flow.  | 
| Netlist Viewer Interface User Guide | 
                             Describes the Netlist Viewer Graphical Interface User Guide that is generic for the stand-alone Netlist Viewer views and the Chip Planner Canvas netlist views.  | 
| SmartDebug User Guide | Describes how to use SmartDebug design debugging tools with PolarFire, SmartFusion2, IGLOO2, and RTG4 devices. | 
| SmartPower User Guide | Describes how to use SmartPower for power analysis. | 
| SmartTime Static Timing Analyzer User Guide | 
                             Describes how to use SmartTime for timing analysis and how to set clock constraints for SmartFusion2,IGLOO2, RTG4, and PolarFire devices.  | 
| Timing Constraints Editor User Guide | Describes how to use the Timing Constraints Editor with timing constraints. | 
| Tcl Commands Reference User Guide for SmartFusion2, IGLOO2, and RTG4 | Lists all Tcl commands and parameters for the Microchip software tools. | 
| SmartDesign User Guide | 
                             Explains how to use the SmartDesign tool, which is used to instantiate, configure, and connect Microchip IPs, user-generated IPs, and custom/glue-logic HDL modules.  | 
| FlashPro Express User Guide | Contains information about how to program your devices using FlashPro Express. | 
| Macro Library User Guide for RTG4 | 
                             Provides descriptions of Microchip library elements for the Microchip RTG4 device family. Symbols, truth tables, and module counts (if appropriate) are included for all macros.  | 
| Macro Library User Guide for SmartFusion2 and IGLOO2 | 
                             Provides descriptions of Microchip library elements for the Microchip SmartFusion2 and IGLOO2 device families. Symbols, truth tables, and module counts (if appropriate) are included for all macros.  | 
| Macro Library Guide for PolarFire | 
                             Provides descriptions of Microchip library elements for Microchip PolarFire device families. Symbols, truth tables, and module counts (if appropriate) are included for all macros.  | 
| PDC Commands User Guide for SmartFusion2, IGLOO2, and RTG4 | Describes the PDC commands for I/O Attributes and Floorplanning constraints with SmartFusion2, IGLOO2, and RTG4 devices. | 
| PDC Commands User Guide for PolarFire FPGA | Describes the PDC commands for I/O Attributes and Floorplanning constraints with PolarFire devices. | 
| User HSM Installation and Setup User Guide | Provides the installation and setup instructions for the User HSM (U-HSM) server. | 
| Secure Production Programming Solution (SPPS) User Guide | Describes the Microchip Secure Production Programming Solution (SPPS), and includes the following information related to High level SPPS overview, use models, software/hardware components of SPPS and tools flow | 
| Job Manager User Guide | Describes how to use the Job Manager to organize manufacturing flow as described in the Secure Production Programming Solution (SPPS) User Guide. | 
| Manufacturer HSM Installation and Setup User Guide | Provides the installation and setup instructions for the Manufacturer HSM (M-HSM) server. | 
| PolarFire SoC MSS Configurator User Guide | Provides the information about PolarFire SoC Microcontroller Subsystem (MSS) Configurator which is a graphical user interface that allows embedded software engineers to define the MSS start-up state quickly. | 
| PolarFire SoC MSS Simulation User Guide | Provides information about the PolarFire SoC MSS simulation which is modeled with Microchip AMBA Bus Functional Model (BFM) to support functional simulation. |