19.4.4.4 Checking Cascaded Math Block Instance Adherence to the Separation Criteria
(Ask a Question)MSVT checks if all of the cascaded Math block instances adhere to the separation criteria. If there are any cascaded Math block instances that violate the separation criteria, then they are listed in the Input signals of the following Math block instances can be observed by failure of config switches in cascade chain section of the report.
Design Example
The following is a chip planner snap shot of a design in which Top_sign21x18_mult_0, Top_sign21x18_mult_1 and Top_sign21x18_mult_2 are three Math blocks. Top_sign21x18_mult_0 is adjacent to Top_sign21x18_mult_1, whereas Top_sign21x18_mult_2 is separated by Top_sign21x18_mult_1 with one MATH cluster.
MSVT Output Report
Because Top_sign21x18_mult_0 is adjacent to Top_sign21x18_mult_1, MSVT fails and reports an error for these MACC instances, as shown in the following. However, asTop_sign21x18_mult_2 is separated from Top_sign21x18_mult_1 by at least one MATH cluster, it is not identified as an error by MSVT, as shown in following report section example.
Input signals of the following Math block instances can be observed by failure of the config switches in the cascade chain
-----------------------------------------------------------------------------------------------------------------------------------------
Input signals of the following Math block instances can be observed by failure of the config switches in the cascade chain: ================================================================================================================== Block1_rom_0/macc_rom_top/MACC_PA_BC_ROM_5/MACC_PHYS_0/INST_MACC_IP of block Block1_rom_0 can be observed by Math block instance Block0_0/block0_level_0/MACC_PA_8/MACC_PHYS_INST/INST_MACC_IP of block Block0_0
-----------------------------------------------------------------------------------------------------------------------------------------