10.1.2 PDC Naming Conventions
(Ask a Question)10.1.2.1 Rules for Displaying Original Names
(Ask a Question)Port names appear exactly as they are defined in a netlist.
Instances and nets display the original names plus an escape character (\) before each backslash (/), and each forward slash (\) is not a hierarchy separator. For example, the instance named A/\B is displayed as A\/\\B.
10.1.2.2 Which Name Do I Use in PDC Commands?
(Ask a Question)When writing PDC commands, follow these rules:
- Always use the macro name as it appears in the netlist.
 - Names from a netlist: 
- For port names, use the names exactly as they appear in the netlist.
 - For instance and net names, add an escape character (\) before each backslash (\) and each forward slash (/) that is not a hierarchy separator.
 
 - For wildcard names, always add an extra backslash (\) before each backslash.
 - Always apply the PDC syntax conventions to any name in a PDC command.
 
The following table provides examples of names as they appear in an imported netlist and the names as they should appear in a PDC file.
| Name and Its Location | Name in the Imported Netlist | Name to Use in PDC File | 
|---|---|---|
| Port name in a netlist | A/:B1 | A/:B1 | 
| Instance name in a netlist | A/:B1 A$(1) | A\\/:B1 A$(1) | 
| Instance name in the netlist but using a wildcard character in a PDC file | A/:B1 | A\\\\/:B* | 
| Net name in a netlist | Net1/:net1 | Net1\\/:net1 | 
When exporting PDC commands, the software always exports names using the PDC rules described in this section.
10.1.2.3 Case Sensitivity When Importing PDC Files
(Ask a Question)The following table lists the case sensitivity in the PDC file based on the source netlist.
| File Type | Case Sensitivity | 
|---|---|
| Verilog | Names in the netlist are case sensitive. | 
| VHDL | Names in the netlist are not case sensitive unless those names appear between slashes (\). | 
For example, in VHDL, capital
            A
         and lowercase
            a
         are the same name, but
            \A\
         and
            \a\
         are two different names. However, in a Verilog netlist, an instance named
            A10
         fails, if spelled as
            a10
         in the set_io command: 
set_io -port_name A10 -pin_name W5 (This command
         succeeds).