4.2.1 Installing a Node-Locked License
(Ask a Question)The following steps describe how to install a node-locked license.
Attention: For UNIX and Linux installations, skip this step and go directly to the Installing a Floating License section.
- Create a folder named FlexLM in a root directory (for example, 
c:\FlexLM), and then save theLicense.datfile in the created folder.Attention: The license file will be attached to the automatically generated email. Alternatively, you can download the license file from the License page at www.microchipdirect.com/fpga-software-products. - 
        Open the Start menu, search for Environment
            Variables.
        The Environment Variables dialog appears.
 - 
        In the dialog, under User Variables, perform the appropriate
          step:
        
If
LM_LICENSE_FILEappears in the dialog:- Select the variable, and then select Edit.
 - 
            Append 
<drive directory>\folder\License.datto the existing value, separating them with a semicolon. - Select OK to save your edits and exit the dialog.
 
If
LM_LICENSE_FILEdoes not appear in the dialog:- Select New.
 - 
            Set the Variable Name to
              
LM_LICENSE_FILE. - 
            Set the Variable Value to 
<drive directory>\Folder\License.dat. - Select OK to save your edits and exit the dialog.
 
 -  Start Libero SoC Design Suite and verify its correct operation.Attention: In the unlikely event you encounter an issue, create a Microchip Support Case.
 
The installation process is complete. You can start using the installed Libero SoC Design Suite tools.