10.2.2 PDC Naming Conventions
(Ask a Question)10.2.2.1 Rules for Displaying Original Names
(Ask a Question)Port names appear exactly as they are defined in a netlist.
Instances and nets display the original names plus an escape character (\) before each backslash (/) and each slash (\) that is not a hierarchy separator. For example, the instance named A/\B is displayed as A\/\\B.
10.2.2.2 Which Name Do I Use in PDC Commands?
(Ask a Question)When writing PDC commands, follow these rules:
- Always use the macro name as it appears in the netlist
- Names from a netlist: For port names, use the names exactly as they appear in the netlist. For instance and net names, add an escape character (\) before each backslash (\) and each slash (/) that is not a hierarchy separator.
- For wildcard names, always add an extra backslash (\) before each backslash
- Always apply the PDC syntax conventions to any name in a PDC command
The following table provides examples of names as they appear in an imported netlist and as they must appear in a PDC file.
| Type of Name and its Location | Name in the Imported netlist | Name to use in PDC File |
|---|---|---|
|
Port name in netlist |
A/:B1 |
A/:B1 |
|
Instance name in a netlist |
A/:B1 A$(1) |
A\\/:B1 A$(1) |
|
Instance name in the netlist but using a wildcard character in a PDC file |
A/:B1 |
A\\\\/:B* |
|
Net name in a netlist |
Net1/:net1 |
Net1\\/:net1 |
When exporting PDC commands, the software always exports names using the PDC rules described in this section.
10.2.2.3 Case Sensitivity When Importing PDC Files
(Ask a Question)The following table shows the case sensitivity in the PDC file based on the source netlist.
| File Type | Case Sensitivity |
|---|---|
|
Verilog |
Names in the netlist are case sensitive. |
|
EDIF (SmartFusion® 2, IGLOO® 2, and RTG4™) |
Names in the netlist are always case sensitive because you use the Rename clause, which is case sensitive. |
|
VHDL |
Names in the netlist are not case sensitive unless those names appear between slashes (\). |
For example, in VHDL, capital "A" and lowercase "a" are the same name, but \A\ and \a\ are two
different names. However, in a Verilog netlist, an instance named "A10" fails, if
spelled as "a10" in the set_location command:
set_location A10 (This command will succeed.)
set_location a10 (This command will fail.)