DRV_ETHPHY_PhyAddressGet Function
C
DRV_ETHPHY_RESULT DRV_ETHPHY_PhyAddressGet(DRV_HANDLE handle, DRV_ETHPHY_INTERFACE_INDEX portIndex, int* pPhyAddress);
Returns
DRV_ETHPHY_RES_OK - operation successful and the PHY address stored at DRV_ETHPHY_RES_HANDLE_ERR - passed in handle was invalid pPhyAddress
Description
This function returns the current PHY address as set by the DRV_ETHPHY_Setup procedure.
Remarks
None.
Preconditions
- The DRV_ETHPHY_Initialize routine must have been called.
- DRV_ETHPHY_Open must have been called to obtain a valid device handle.
- DRV_ETHPHY_Setup must have been called to properly configure the PHY