DRV_ETHPHY_ClientStatus Function
C
DRV_ETHPHY_CLIENT_STATUS DRV_ETHPHY_ClientStatus(DRV_HANDLE handle);
Returns
- DRV_ETHPHY_CLIENT_STATUS value describing the current status of the driver.
Description
This function gets the client-specific status of the Ethernet PHY driver associated with the given handle.
Remarks
This function will not block for hardware access and will immediately return the current status. This function has to be used to check that a driver operation has completed. It will return DRV_ETHPHY_CLIENT_STATUS_BUSY when an operation is in progress. It will return DRV_ETHPHY_CLIENT_STATUS_READY when the operation has completed.
Preconditions
- The DRV_ETHPHY_Initialize routine must have been called.
- DRV_ETHPHY_Open must have been called to obtain a valid opened device handle.
}